PLCopen State Machine
- This combination of motion profiles is useful in building a more complicated profile or in handling exceptions within a program The act of performing a sequence of instructions or commands..
- In real implementations there can be additional states defined at a lower level.
- The basic rule is that motion commands are always taken sequentially, even if the PLC Programmable Logic Controller - A digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events. has the capability of real parallel processing.
- These commands act on the state diagram of the axis.
- The axis is always in one of the defined states.
- A change of state is reflected immediately when issuing the corresponding motion command.
- The response time of immediately is system dependent.
The defined seven states are:
- Continuous Motion
- Discrete Motion
- Error Stop
- Homing The homing procedure allows, based on a position measurement, to set a position offset to the motor to ensure it is physically at the home position.
- Stand Still
- Stopping
- Synchronized Combines an axis or axes group (as slave) with an axis as master. The slave executes its path with synchronization to the progress of the master. This is linked to a one dimension source for synchronization. Motion
Figure 1: Motion State Machine (PLCopen)
Notes
- In the ErrorStop or Stopping state, all function A function calculates a result according to the current value of its inputs.
A function has no internal data and is not linked to declared instances. blocks can be called, although they are not executed.
The exceptions are MC_Reset New start of the microprocessor. and Error which generate the transition to StandStill or ErrorStop respectively. - MC_Power FB is called with Enable=TRUE and there is an error in the Axis.
- MC_Power FB is called with Enable=TRUE and there is no error in the Axis.
- MC_Stop.Done and not MC_Stop Execute.
State Machine for Multi-axes Motion Control
The diagram is focused on a single-axis.
- The multi-axes function blocks (e.g., MC_CamIn, MC_GearIn, or MC_Phasing) can be looked at, from a state diagram point of view, as multiple single-axes all in specific states.
- Example: The CAM-master can be in the state Continuous Motion.
- The corresponding slave is in the state Synchronized Motion.
- Connecting a slave axis to a master axis has no influence on the master axis.
A normal procedure starts in StandStill.
- In this state the power can be switched on per axis (via the MC_Power command).
- Access the Homing state (via the issue of the command Home per axis).
This returns to StandStill after normal completion. - From here, transfer an axis to either Discrete Motion or Continuous Motion.
- Via the Stopping state you can return to StandStill.
- ErrorStop is a state to which the axis transfers in case of error.
- Via a (manual) MC_ResetError command, return to StandStill.
- From this state, the machine The complete assembly of all connected parts or devices, of which at least one is movable. can be moved to an operational state again.
- Access the Homing state (via the issue of the command Home per axis).
The States define the functionality of the function blocks.
- Function Blocks not listed in the State Diagram do not affect the state of the axis.
- This means that, whenever they are called, the state does not change.
- They are:
Disabled State
The Disabled Removal of the ENABLE signal. Disables power stage. state describes the initial state of the axis.
Disable means power off without error.
- In this state, the movement of the axis is not influenced by the FBs.
- The axis feedback is operational.
- If the MC_Power FB is called with Enable=TRUE while being in Disabled, this leads to either:
- Standstill if there is no error inside the axis.
- ErrorStop if an error exists.
- Calling MC_Power with Enable=FALSE in any state, the axis goes to the state Disabled, either directly The orientation components of a vector in space. or via any other state.
- If a motion generating FB controls an axis while the MC_Power FB with Enable=FALSE is called, the motion generating FB is aborted (CommandAborted).
ErrorStop State
The ErrorStop state is the axis goes to a stop, if possible.
- No further FBs are accepted until a reset has been done from the ErrorStop state.
- The transition Error refers to errors from the axis and axis control, and not from the function block instances.
- These axis' errors are reflected in the output of the function blocks FB instances errors.
- Issuing MC_Home in any other state than StandStill goes to ErrorStop, even if MC_Home is issued from the Homing state itself.
- ErrorStop is valid as highest priority and applicable in case of an error.
- The axis can have either power enabled Enable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive. or disabled, and can be changed via MC_Power.
- However, as long as the error is pending, the state remains ErrorStop.
From StandStill to Stopping
StandStill is power on without an error.
- Calling the FB MC_Stop in state StandStill changes the state to Stopping and back to Standstill when Execute = FALSE.
- The Stopping state is kept as long as the input Execute = TRUE.
- The Done output is set when the stop ramp The gradual acceleration and deceleration of a stepping motor. This is essential if performance beyond the start/stop range is required. The slope of the ramp is a function of screw pitch, load, drive voltage and design, and motor. is finished.